This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25790: Current limit meeting EN62368-1 standard

Part Number: BQ25790


Does the BQ25790 guarantee that it meets the requirements of "current limiting IC" as specified in G.9 of the European safety standard EN62368-1?

In the verification of a single fault condition in the European safety standard, a short circuit on each terminal of each component must be verified.
We want to prevent the USB PD from flowing 5-20V, up to 3A, into the battery or circuit due to a short circuit.
If a component is defined as a "current-limiting IC" as defined in section G.9 of the safety standard, is there a recognition that the component does not have to take short circuits into account in accordance with the regulations?