This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I am writing to request a SPICE model for the TPS5405DR voltage regulator. As we are in the process of simulating our circuit design, having access to the SPICE model will help us in continuing simulation for EMI/EMC Project. Could you please provide us with the SPICE model for the TPS5405DR .
Thanks, and Regards
Chandana Patil
Hi Chandana
Sorry that TPS5405 has no spice model available. Will you consider the TPS54202 ? It's 4.5V-28V, 2A output, SOT23-6 package, internal compensation, adjustable output.
The spice model is available on ti.com. https://www.ti.com/product/TPS54202#design-development
Thanks and best regards.
Thank you for your suggestion. But the model you suggested has a fixed switching frequency of 500KHz and model we are looking for is adjustable, the maximum switching frequency of the model is 1.1 MHz Your suggested model doesn't match exactly. Even pin configuration is different. We are trying to study both the models and will update you. It will be helpful if you suggest as any model that will match with our model (TPS5405).
Thanks, and Regards
Chandana Patil
Hi Chandana
Sorry that I didn't find spice model which has match pin with TPS5405, please let me know if you got any updates from your side. Thank you!