This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7310: Paralelling 2 power supplies

Part Number: LM7310
Other Parts Discussed in Thread: TPS25947,

Hello,

I want to put in parallel 2 power supplies with output of 12V/4A in order to supply a load of 12V/8A.

I want that bout power supplies supply current at the same time (not ona supplying and the other in standby).

Can I use LM7310 or TPS25947 for this purpouse? Which is the difference between them?

Thanks,

Marina