This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2576S-ADJEVM: LM2576S-ADJEVM

Part Number: LM2576S-ADJEVM
Other Parts Discussed in Thread: LM2576

Hi TI Team,

In our design we are using LM2576S-ADJ/NOPB part, I am unable to get WEBENCH® Designer  for LM2576S-ADJ/NOPB.

Can you please suggest Cout and inductor values ?

Input voltage range= 10V-28V

Input capacitor Cin= 2, 220uF @ 180mOhm input capacitors.

We are striving for 2 years of life at 70 ambient.  With 2, 220uF capacitors and Vout  5V @1.3A DC load current results in a 0.78A ripple at 52kHz on the input capacitor...estimate. 

Re-evaluate the inductor and output capacitors based on the new limitations ?