This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-R2: Configuring Data Flash Memory.

Part Number: BQ34Z100-R2

Hello ,
I have some problems by configuring data flash memory . 

 If I set volt scale , current scale or energy scale values to a value that the different from "1" , do i have to scale all other values that in units mAmp, mAmpHr, mVolt , mW,cW ?  


Example1: 

Before ==> Volt Scale  = 1   ,    Cell Taper Voltage = 100 mV   

After ==>    if Volt Scale = 10 , Cell Taper Voltage = 10 mV. 

Example2: 

Before ==> Current Sclae = 1 , Taper Current = 140 mA   

After ==>    if Current scale = 10 , Taper Current = 14 mA . Is this correct ?