Hi Team,
In my customer charger application, they have 2 power input sources from USB or Qi. The TPS2120 could be used for the input source switching and OVP/OCP protection for the USB input.
I would like to check with you that if it is possible to set the OCP current limit to be lower than 1A by using a RLIM > 100kOhm?

Their USB max current is <500mA, ideally, zthey want to set the current limit to be close to 500mA.
Best Regards,
Ernest