This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22916: Part recommendation

Part Number: TPS22916

Hi team,

Could you help check if we get recommendation meet following spec requirement?

Load Switch

 

 

3.6V

VDD

1.0V ~ 5.5V

 

Vout

0V ~ 5.5V

 

RON

Max.50m ohm

 

ISW

Max. 2.0A

 

Iq (EN=0)

Max. 0.65uA

 

tON(Turn On Time)

Min. 0.18 ms

 

En VIH

Min. 1.2V

 

En VIL

Max. 0.4V

Thanks and Best Regards,

Will