This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS35: Device recommendation

Part Number: TPS35


I am looking for a watchdog timer or some kind of counter that can time-out if a fan tachometer stops toggling.

 

This part below looks good. I was hoping to get a smaller package that SOT-23

TPS35 data sheet, product information and support | TI.com

 

The WSON version is low inventory. Does TI has a part like this in small package?

I would prefer adjustable, but I need:

  • Watchdog-style time-out
  • 1 s (aprox)
  • No need for a start-up delay
  • Reset pin
  • WDI reset pin on falling edge