Hi
When the input voltage is adjusted from 5v to 25v, the following products Will the frequency drop? How to set the inductor?
TPS56387
TPS51386
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What's your output voltage? you can refer to below table to select the inductor. Thanks.
Aurora
Hi,
Frequency reduction will occur during light load to improve light load efficiency. No frequency reduction when under heavy load or full load. When designing the inductor, it should be designed according to the output current and frequency at full load. Thanks.
Aurora