Hi,
We are controlling the pin MR of TPS3808 with a MOSFET. But, the leak into the transistor make the MR pin to trig because of the drop into the MR pull-up resistor. This occur only when we are testing the circuit in high temperature. Our current MOSFET is leaking up to 10uA at high temperature, this lead to a drop at MR pin that is enough to activate the MR pin.
So we were wondering if it is possible to know the maximum pull-up resistance of MR so we can find the good MOSFET with a leak that fit with the maximum pull-up resistor of MR pin.
We don't want to add a weaker pull-up in parallel with MR because we want to be low power as possible.