I would like TI engineering assistance for a new HVAC project my company, ACTA-TechUS, is implementing. It will make substantial use of TI semiconductors in the power supply and related control systems. Our intention is to design the hardware using all US made components and parts.
The system will require an operating DC voltage of between 90 V dc and 110 Vdc that will be derived from the 110 VAC 60Hz power line. Our design goal is to build a Transformer-less power supply using a capacitive coupled design. We have done this before on a power supply delivering 36Vdc and 750 mA. With the HVAC system we will require the DC voltage at up to 15 Amps.Triacs, Thyristors
We have some of the potential circuit designs and I would like to recruit the assistance of the TI engineering group to select the appropriate TI components and help us design them into the system. The current design uses these types of components: Triacs, Thyristors, Optocoupler and standard semiconductors, diodes etc.
Please have someone from the engineering group contact me to create a plan.
Peter Kaufman, CTO
ACTA-TechUS, Inc.
6121 183rd Street
Fresh Meadows, NY 11365-2114
(718) 445-0038
info@actaitechus.com or pkaufman@d2ir.com