Can we use Iadj pin to enable constant voltage (CV) operation by modulating the constant current level when the output voltage reaches a maximum value?
I would like to use TPS92691 as a CC/CV charger for 36V battery in a boost converter configuration with Vin= 22V. I was thinking in using an external feedback circuit from Vout in order to modulate or adjust the voltage of Iadj pin such that the output current is gradually decreased versus Vout when the Vout hits a predetermined level.
Is it possible?