Part Number: TPS259827LEVM
Other Parts Discussed in Thread: TPS25982
HI,
Recently, we encountered some problems when testing whether TPS259827LEVM meets our needs and need your help.
--
When we tested, we used the public version for testing, and the backend was connected to the Electronic Load.
Electronic Load is used to simulate the inrush part, so before the TPS259827LEVM is powered on, the Electronic Load will be kept on. At this time, after the TPS259827 is powered on, it will fail to start.
CdVdt is the only part that can control the inrush slew rate according to specifications. Even if I adjust it to a high value or open, I still can't solve the problem.
If you change the order of opening, turn on Power first and then Electronic Load, the working status will be normal.
Test conditions:
1.Electronic Load CC Mode, current 9A.
2.TPS259827LEVM CdVdt:Open.
--
When observing the waveform, assuming I set 9A, the protection will trip immediately after the current rises to 9A.
Currently, the public version and Electronic Load are not connected to any RL.
Therefore, my preliminary analysis is that this architecture is a purely capacitive circuit. It does not start the dvdt at the beginning, but enters the current limit.Then the device is triggered going into thermal shutdown during startup.
So I would like to ask if it can be solved by adjusting the resistor at the output end? If it can be solved, what role does RlStart play in this system? What value does RlStart usually take? Will there be any impact if the size is too large?
Also, I would like to ask, thermal shutdown is the protection component of the IC. The protection should be triggered regardless of output and input. The output can be adjusted using Cdvdt. What about input?
Please help to reply to this question.Thanks.