This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131-Q1: Request a schematic review.

Part Number: TPS65131-Q1


Hi

The circuit diagram was designed with the following specifications.

-SPEC-

Input: DC 2.7~5.5V

Output: DC +12.9V / -12.9V, 1.7A

Frequency:1.38Mhz


Please review the attached circuit diagram.

Thanks