Other Parts Discussed in Thread: LM74800-Q1,
Dear TI team,
In my design i am using LM7481 as Oring circuit and reverse current blocker. My circuit has a battery which is activated during main power supply failure. In my tests, i am realizing power failure by cutting the 28V main input using a switch and the power goes down almost in 400us enabling battery. But, when battery is enabled, Q1 gate-source voltage goes low in almost 1.5ms resulting in reverse current flow into main power supply and disabling battery. As result my power supply is interrrupted and the test has failed. From the power management forum i have seen that LM7481 detects reverse current by measuring C pin to A pin voltage level and if it exceeds -5.5mV threshold the ic shuts down Q1. But until then it allows a reverse current flow. I am using a mosfet which has 2.2mohm on resistance. As i understood, it is needed almost 2.5A reverse current before the mosfet is turned off to block reverse current?
In my design i am using the reference circuit in the datasheet page-16, figure 9-1, except VOUT2 output.
Could you please give me information about this reverse current property more detailed? And also could you please justify my findings about threshold for fast reverse current blocking voltage which is needed for Q1 to be shut down?