Other Parts Discussed in Thread: TPS2514,
Hello,
I am trying to charge both an iPhone and an Android Smartphone with a simple desk power supplier.
I have a simple PCB that is able to connect the 4 cables V+, DP, DN and GND to a USB-C connector.
The V+ and GND are connected to the 5V power supplier able to provide up to 3A.
All the 4 cables are also connected to the TPS2514 chip to allow the smartphones to work correctly.
The Android Smartphone is requiring 1.5A (I thought that with this chip I could use the fast charging up to 2.4A).
The iPhone is continuously switching the current when it is switched off between0.46A (when showing the charging icon) and 0.3A when not showing it (like 7s with the icon and 1s without it).
As soon as the iPhone switches on, the current goes down to 0.02A and the smartphone switches off again.
I wasn't expecting this behavior.
Can you please help me understanding how to correctly handle the charging of both smartphones?
Thank you very much.