Can you tell me what the max junction temperature rating is for TPS3306-18D and the case to junction resistance? These are not specified on the datasheet.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you tell me what the max junction temperature rating is for TPS3306-18D and the case to junction resistance? These are not specified on the datasheet.
Hi Zach,
It is 85C.
Jesse
Can you explain more. 85C is also the ambient temperature rating for the part. Usually the junction temperature is higher than the ambient temperature rating. I'm used to seeing parts like this have a max junction temperature of +125C with an ambient temperature of +85C.
Hi Zach,
Since this device has a low power dissipation, it can be assumed that T(junction)=T(ambient).
Jesse