This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76952: Cannot I2C communicate after FET_EN set.

Part Number: BQ76952
Other Parts Discussed in Thread: BQSTUDIO, EV2400

Hi Team,

I'm trying to manage 7s-Lib with stand-alone bq76952.
However as soon as I set FET_EN, I lose I2C communication with bqStudio(v1.3.101 or v1.3.124).
It seems the frequency of SCL goes fast after set that bit.
The amplitude looks OK(2.5V).
I use handmade EV2400 to communicate.
And I attach a part of the gg.csv file which has not set FET_EN.
Please give me some advice.

Regards,
Makoto Teramoto

"Settings","Fuse","Min Blow Fuse Voltage","5000","mV"
"Settings","Fuse","Fuse Blow Timeout","30","s"
"Settings","Configuration","Power Config","2181","Hex"
"Settings","Configuration","REG12 Config","9f","Hex"
"Settings","Configuration","REG0 Config","01","Hex"
"Settings","Configuration","HWD Regulator Options","00","Hex"
"Settings","Configuration","Comm Type","11","—"
"Settings","Configuration","I2C Address","00","—"
"Settings","Configuration","SPI Configuration","20","—"
"Settings","Configuration","Comm Idle Time","0","s"
"Settings","Configuration","CFETOFF Pin Config","00","Hex"
"Settings","Configuration","DFETOFF Pin Config","00","Hex"
"Settings","Configuration","ALERT Pin Config","00","Hex"
"Settings","Configuration","TS1 Config","07","Hex"
"Settings","Configuration","TS2 Config","00","Hex"
"Settings","Configuration","TS3 Config","0f","Hex"
"Settings","Configuration","HDQ Pin Config","00","Hex"
"Settings","Configuration","DCHG Pin Config","00","Hex"
"Settings","Configuration","DDSG Pin Config","00","Hex"
"Settings","Configuration","DA Configuration","05","Hex"
"Settings","Configuration","Vcell Mode","80af","Hex"
"Settings","Configuration","CC3 Samples","80","Num"
"Settings","Protection","Protection Configuration","0602","Hex"
"Settings","Protection","Enabled Protections A","bc","Hex"
"Settings","Protection","Enabled Protections B","f3","Hex"
"Settings","Protection","Enabled Protections C","70","Hex"
"Settings","Protection","CHG FET Protections A","18","Hex"
"Settings","Protection","CHG FET Protections B","d1","Hex"
"Settings","Protection","CHG FET Protections C","10","Hex"
"Settings","Protection","DSG FET Protections A","a4","Hex"
"Settings","Protection","DSG FET Protections B","e2","Hex"
"Settings","Protection","DSG FET Protections C","60","Hex"
"Settings","Protection","Body Diode Threshold","50","mA"
"Settings","Alarm","Default Alarm Mask","f800","Hex"
"Settings","Alarm","SF Alert Mask A","fc","Hex"
"Settings","Alarm","SF Alert Mask B","f7","Hex"
"Settings","Alarm","SF Alert Mask C","f4","Hex"
"Settings","Alarm","PF Alert Mask A","5f","Hex"
"Settings","Alarm","PF Alert Mask B","9f","Hex"
"Settings","Alarm","PF Alert Mask C","00","Hex"
"Settings","Alarm","PF Alert Mask D","00","Hex"
"Settings","Permanent Failure","Enabled PF A","03","Hex"
"Settings","Permanent Failure","Enabled PF B","00","Hex"
"Settings","Permanent Failure","Enabled PF C","07","Hex"
"Settings","Permanent Failure","Enabled PF D","00","Hex"
"Settings","FET","FET Options","0b","Hex"
"Settings","FET","Chg Pump Control","01","Hex"
"Settings","FET","Precharge Start Voltage","0","mV"
"Settings","FET","Precharge Stop Voltage","0","mV"
"Settings","FET","Predischarge Timeout","5","10ms"
"Settings","FET","Predischarge Stop Delta","500","mV"
"Settings","Current Thresholds","Dsg Current Threshold","100","userA"
"Settings","Current Thresholds","Chg Current Threshold","50","userA"
"Settings","Cell Open-Wire","Check Time","5","s"
"Settings","Interconnect Resistances","Cell 1 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 2 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 3 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 4 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 5 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 6 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 7 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 8 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 9 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 10 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 11 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 12 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 13 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 14 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 15 Interconnect","0","mΩ"
"Settings","Interconnect Resistances","Cell 16 Interconnect","0","mΩ"
"Settings","Manufacturing","Mfg Status Init","0040","Hex"
"Settings","Cell Balancing Config","Balancing Configuration","17","Hex"
"Settings","Cell Balancing Config","Min Cell Temp","-20","°C"
"Settings","Cell Balancing Config","Max Cell Temp","60","°C"
"Settings","Cell Balancing Config","Max Internal Temp","70","°C"
"Settings","Cell Balancing Config","Cell Balance Interval","20","s"
"Settings","Cell Balancing Config","Cell Balance Max Cells","2","Num"
"Settings","Cell Balancing Config","Cell Balance Min Cell V (Charge)","3900","mV"
"Settings","Cell Balancing Config","Cell Balance Min Delta (Charge)","20","mV"
"Settings","Cell Balancing Config","Cell Balance Stop Delta (Charge)","10","mV"
"Settings","Cell Balancing Config","Cell Balance Min Cell V (Relax)","3900","mV"
"Settings","Cell Balancing Config","Cell Balance Min Delta (Relax)","20","mV"
"Settings","Cell Balancing Config","Cell Balance Stop Delta (Relax)","10","mV"
"Power","Shutdown","Shutdown Cell Voltage","2000","mV"
"Power","Shutdown","Shutdown Stack Voltage","6000","mV"
"Power","Shutdown","Low V Shutdown Delay","1","s"
"Power","Shutdown","Shutdown Temperature","85","°C"
"Power","Shutdown","Shutdown Temperature Delay","5","s"
"Power","Shutdown","FET Off Delay","0","0.25s"
"Power","Shutdown","Shutdown Command Delay","0","0.25s"
"Power","Shutdown","Auto Shutdown Time","0","min"
"Power","Shutdown","RAM Fail Shutdown Time","5","s"
"Power","Sleep","Sleep Current","20","mA"
"Power","Sleep","Voltage Time","5","s"
"Power","Sleep","Wake Comparator Current","500","mA"
"Power","Sleep","Sleep Hysteresis Time","10","s"
"Power","Sleep","Sleep Charger Voltage Threshold","20000","mV"
"Power","Sleep","Sleep Charger PACK-TOS Delta","2000","mV"