Hi there,
I am using TPSM63610 in my project for three applications (28V to 12V, 28V to 8.5V and 12V to 4V conversion). In the datasheet (reference schematic in the datasheet) as well in TI WEBENCH circuit designer, the IC is being enabled through Vin only. I would like to know it is possible to enable the IC using a FPGA signal. If yes, kindly share the reference schematic for the same.