This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25750: Use multiple charger

Part Number: BQ25750

Hello,

I need to develop a DC/DC converter that can provide 60A current output. Is it possible to put 3 BQ25750 converters in parallel to reach 60A?

The datasheet indicates that the converter requires a 5mohm shunt. is it possible to put a shunt 3 times smaller to reach the 60A?

Best Regards

Ludovic Micou