This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61197: I2C to PWM converter

Part Number: TPS61197

Hello,

We're looking for an I2C device with a small number of PWM outputs. It needs to have 0 - 98% duty cycle range and an operating frequency that extends down to 1kHz or (preferably) lower. The application is to drive the PWM input of the TPS61197. Does anyone know if such a device exists in the TI range? We could use the on-board micro but there might be a problem with maintaining stability of the PWM as the micro is doing quite a lot of other work!

Thanks