Hi,
i am really confused here. For sometime, i was thinking using TPS54260 as an inverting buck boost and now, i found out that the output current is not the rated current of the TPS542560 (2.5Amps) . the real output of the device is decreased by (1-Duty cycle).
Can i use "TPS40170 " to generate a negative 15V using 'inverting buck-boost topology'? my requirement is Vin-min=19V, Vin _max=45V, Output voltage=-15V, iout=2.5A. is there an application note that will help me to design it?
Thank you
Sara