This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB-PD-CHG-EVM-01: Integrated USB-PD Source IC w/ Buck

Part Number: USB-PD-CHG-EVM-01
Other Parts Discussed in Thread: BQ25756, BQ25756E, TPS25751, BQ25620, BQ25798

Hello,

I would like to add USB / USB-C charge-only (source) ports to a project with existing DC supply rails. It is difficult to sort through all of the options for various USB-PD topolgies, and I would appreciate if someone could point me in the right direction.

I am looking for a standalone IC that can accept 20-30VDC input, and provide USB-PD negotiation and voltage regulation to the sinking device(s). The goal is a low parts count. I would be interested if there are any dual-channel options. Thanks!