This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ35100: Gauging Lithium Thionyl Chloride chemistry Battery package

Part Number: BQ35100

Hi,

          I'm using Bq35100 for gauging the battery pack in which 12 cells are connected in parallel. The chemistry of my cell is Lithium Thionyl Chloride. Each cell is of capacity 17Ah. This makes the total capacity 204Ah,whcih can be stored in a 4 bytes variable.But the gauge is showing that the design capacity can be maximum of 2 bytes. Then what value can be written as the cell design capacity?...