Other Parts Discussed in Thread: SN6501-Q1
We want to drive the LMG5200's high-side gate with a PWM duty close to 100%. More specifically, every ten milliseconds, we wish to turn the high-side gate off for a microsecond or less.
After inspecting the datasheet, we understand that the device's bootstrap supply will not be able to support this operating mode. Because of this, we have considered connecting an isolated DC-DC converter to the device's HS and HB terminals. However, we are unsure how to do this in a way compatible with this device.
In another LMG5200 discussion, it is stated that the device's bootstrap has an internal switch that only allows its internal capacitor to be charged to the required voltage. Therefore, could an isolated DC-DC converter with a 6V output be connected across the device's HS and HB pins, with a resistor used to limit current flow?
Is there any technical literature published by TI that describes the best way to achieve this?