Other Parts Discussed in Thread: LM317,
Using TLV70450DBVR SOT-23-5 for 5V out at up to 150mA with 5.5-11V in.
We are needing 6V out, and cannot find a part with pinout close to this. Pin 1=GND is an odd part. A lot of ths SOT-23-5 use pin 4 and 5 as input and output.
1. Can you help us find a pin compatible part ? (I found TPS709B50 has same poinout, but there is no 6V part), TPS70960 has different pinout)
2. If not, can we use this as an adjustable to get 6V (like typically used on the LM7805)...
Thanks