This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can TPS54260 support Vin=+25V, Vout-24V, Iout = 750mA?

Other Parts Discussed in Thread: TPS54260

I need -24 V @ 750 mA for my application. My Vin is going to be 25V. Can the TPS54260 be used as an inverter in this case and give me the desired output? If not is there any other TI device which might work? I really appreciate your help!

 

regards,

 

Sushant