This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7705: Automotive Equivalent

Part Number: LM7705

Hello,

LM7705 is a very commonly recommended device with op amps to get true swing to 0V on the output. I was looking for an equivalent automotive device and didn't see one. Is there a good similar or equivalent device to the LM7705 that is automotive grade?

Best,
Jerry

  • Hi Jerry,

    We do not have an Auto equivalent for LM7705.

    The Auto grade Charge Pump in our portfolio would be TPS6040x-Q1. However, this is an unregulated Charge Pump and the minimum negative voltage would be -1.8V with this Charge Pump.

    Regards,

    Febin