Other Parts Discussed in Thread: LM5176, LM5177
Hi.
I want to use LM5175 in boost mode.
The H/W configuration environment is as follow.
- Input Power: 12-16.5V (Battery Power), (12V*6A)*(4 Battery Pack Parallel) = 288W
- Output Power: 24V@280W
- Q1: Is a 280W power design possible with a single LM5175 configuration?
- Q2: please tell me the maximum output.
- Q3: Can I configure LM5175 in parallel and use it as on load?
I will wait for your reply. Thanks for your help.
- Jungsik kwak