This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: overheat during soft start.

Part Number: TPS2660
Other Parts Discussed in Thread: TPS1663

Hi BU friend,

Here is a requirement from customer of Efuse:

1.The input of the device is a 12S battery, with a maximum voltage of 50.4V and a minimum voltage of 26V; the maximum operating current is 2A;

2. Equipped with over-current protection function, the protection threshold is about 4A. With short circuit protection function.
3. Compatible with large capacitive loads, the capacitance is tentatively set at 200uf.

I learned about efuse, such as TPS2660, and used the calculation tool on the official website to calculate it. The main problem of this device is that it will overheat during soft start.
Are there any other suitable devices to recommend?