This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92830-Q1: How to prevent LED flash at startup?

Part Number: TPS92830-Q1
Other Parts Discussed in Thread: TPS92623-Q1

Hi, I am using this device to drive an RGB LED. I am not using the internal PWM generator, but providing PWM from a microcontroller. On power-up, the LED flashes white. Is there a way to prevent this from happening? The PWM inputs are low during power-up. Thanks.

  • Hi Henry,

    Could you provide the schematic for your application and the test waveforms of SUPPLY, G1/2/3 and so on?

    In addition, what are your detailed application requirements, like current, output voltage, frequence and duty cycle?

    since you are not using the internal PWM generator, if the current is not high, TPS92623-Q1 could be an easy option.

    BR,

    Hailee.