Hi Application team:
My customer has design in LM63460AASQRYFRQ1 from 24V to 12V .
but customer is tested Input current consumption is around 2mA(Vin=12.3V) to 6mA(Vin=24V) without load current (Iout=0A) in PFM mode cannot meet the design spec . I have two questions , could you please help give comments?
(1) Base on the spec Quiescent current (7uA / 10ruA typ with Vout=3.3V/5V) , if we need meet ~uA spec , May I know the only way is need change FB pull high resistor RFBT to 1Mohm and fine tune the FB pull down resistor to reduce input current consumption?
(2) If design spec Vout=12V from Vin=16V to 36V with no load (Iout=0A). Will the input quiescent current same as the spec definition as above question 1 ?
Schematic as below attachment
(1) Vin min = 16V
(2) Vin typ = 24V
(3) Vin max= 36V.
(4) Vout =12V with +/-5% tolerance.
(5) Iout= 0A test input quiescent current
(6) SW freq ~ 2.07MHz (Auto mode)