Dear TI:


一、In TPS562200DDCR datasheet Recommended Operating Conditions,as shown in the left figure,There are two parameters for Operating temperature:TJ:-40 to 150℃ and Recommended Operating free-air temperature is -40 to 85℃.So ,Is these two requirements need to be met at the same time?Or as shown in the right figure ,In the condition of TJ<125℃ and free-air temperature=100℃ ,the ic performance can be guaranteed?
二、In TPS562200DDCR datasheet,as shown in the bottom figure,Operating junction temperature is -40 to 125℃ ,So,what is the free-air temperature required?As TPS562200DDCR and
TPS562201DDCR Maximum Operating junction temperature is same of -40 to 150℃。What's the difference between them?

Looking forward to your reply,thank you!