What are the package dimensions of the TPS84620? Specifically the height of the package. We need something that is very low profile on the order of 3mm or less. The datasheet is not yet available so I cannot verify.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
That data sheet is on the web...The height is 2.8 +/- 0.1 mm.
Hi Jimmy,
Please note that the TPS84621 has a wider output voltage range, down to 0.6V. This is fully released and is completely pin-to-pin compatible with the TPS84620, and the same height dimensions.
http://www.ti.com/product/tps84621
Regards,
Colleen