Part Number: TPSM365R6
Is this able to support IBB topology for 24Vin to -15V/200mA?
Is there similar design with power module? thanks.
Regards
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPSM365R6
Is this able to support IBB topology for 24Vin to -15V/200mA?
Is there similar design with power module? thanks.
Regards
Brian
Hello Brian,
My colleague will provide his advice to you shortly.
Hi Brian,
The TPSM365R6 device will only work with up to -13 V of output voltage in an IBB configuration. This is due to the non-IBB version only being able to output 13 V max.
However, the TPSM5601R5H should be able to support this IBB application at 24 VIN and -15V/200mA out. Please see this application note for more details.
There is also an IBB EVM for this part if you want to evaluate the device that way.
Thank you,
Joshua Austria