This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28951: Can it do 390V in and +/-120V out 10 A?

Part Number: UCC28951

Hi 

Can UCC28951 take in 390V DC and convert it to two power rail +120V and -120V 10A ? 

  • Hello,

    Your inquiry is under review and I will get back to you shortly.

    Regards,

  • Hello,

    A phase shifted full bridge (PSFB) using the UCC28951 can be designed for the power range that you have described.

    Since the power is so high for each rail you want to design two power stages for each real and interleave them.

    This will cut the conduction losses is half and reduce the total magnetic size by up to 33%.  This will also decrease the RMS currents in the input and output capacitors.

    The following link will bring you to an application note that describes how to design a single stage PSFB using the UCC28951.  There is a link to an excel design tool that goes along with it.

    https://www.ti.com/lit/pdf/slua560

    If one to do it with one phase you could use two center tapped secondary winding for the +/- 120 V outputs.  The excel design tool and app note previously motioned is applicable for both stages.

    Regards,