This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5164: SW signal abnormal

Part Number: LM5164

Hi team, could you help to check if the waveform is normal? it seems the signal of SW pin has a rush down.

  • Hello Jingguo,

    The waveform taken appears to be at light load and its converter is running in DCM operation.  The first on pulse occurs in which inductor current rises, the on pulse is not enough to charge the output above the reference voltage at the feedback, and therefore  this is followed with a second pulse that charges the output above the reference, then this is followed by a period of time in which the inductor current goes to zero amps and meanwhile the output voltage is still above the reference in which the next on pulse will not happen until feedback voltage equals the reference voltages.  Sometimes at light loads, the switching behavior can look like this and its normal.

    Hope this helps.

    David.