Hi
I'm Frank
we met some problem for LM5122MHX used for LOW SIDE BUCK (as custermer requirement as Charger) Input 56V output 53.5V/10A
there is some question below
1. would you give me some advice if you have experince LM5122MHX on the Low-side buck schematic ?
2. when we use Master schematic W/O Slave it seems could be load to 2A continue (Target is 5A per Phase) , but when we use the 2- phase (Master/Slave),it seem board will Damage
but we dont know how...
So if you have any idea/tips that maybe you could share to us
Below is Master/Slave/Loop/Waveform