Hi,
Can you please send me a reference design for using TPSM64406 for Dual Negative Outputs.
In my design the input is 24VDC and there are two outputs -15VDC,1A and -12VDC,1A.
Thanks,
Eyal
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Can you please send me a reference design for using TPSM64406 for Dual Negative Outputs.
In my design the input is 24VDC and there are two outputs -15VDC,1A and -12VDC,1A.
Thanks,
Eyal
Hi Eyal, I think this is possible, but, the voltage stress you would be exerting on the device is VIN + abs(VOUT1,2) = 39V.
The device can only operate to 36V max.
Could you consider a flyback design for this application?
https://www.ti.com/product/LM25184
There is a quick start calculator here to help you with your design