Other Parts Discussed in Thread: TPS25750
Dear TI,
when will be available reworked/repaired version of TPS25751 please? Is it available already to order new version through samples, please?
thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jan,
The TPS25751 should start sampling soon, within the next couple weeks.
Thanks and Regards,
Chris
Hello Chris,
thank you. You told us, it will be available in April. We are under a pressure with time release of new product and we are only waiting on this part, which was recommended by TI because previous models had bugs and issues with functions, which should work and did not. This model also had a bugs, which you told will be solved in final part, which release time is beginning of April.
So any more exact lead time of the final, bug free part, is very appreciated. Just a "couple of weeks" is not an answer we need after months of waiting. Thank you for understanding our position.
Waiting for mode deteailed information about current status.
Thank you a lot.
Jan
Hi Jan,
I can help step in here. First off, apologies for the difficulties you had in your migration over to the TPS25751 from the TPS25750.
For the release of the device, all of the content currently available on ti.com is the final version. For example, the datasheet, user guides, application customization tool, etc.. are all finalized for our full release on ti.com. The only thing we are currently waiting on is the production marked material to be stocked on the ti.com store. This was originally scheduled for end of March, but there were unfortunately some delays in the manufacturing that have pushed us into April. However, it is in final steps of our manufacturing process which is why we are confident it will be stocked within these next couple of weeks.
If you are waiting to go into full production, you will need to wait for the production marked material to be stocked on ti.com. However, if this is for internal engineering builds then you can leverage the samples that are currently available on the ti.com store. You do not need to wait until the production marked material is stocked on the web.
If you are using this pre production marked material already, is there a specific issue that you are still seeing? Our team can help try to resolve this issue