When I power on my board, the UCD9248 sometimes refuses to start regulating. I can communicate with the device over PMBus. In the Fusion Digital Power Designer GUI, I can see that POWER_GOOD# is asserted. The GUI also reports a Vin reading of 0.790 V, but Vin is acually at 12V. When I measure on the TMUX outputs on the UCD9248, they are all constantly high. It seems like the device sometimes latches up somehow. Most of the times it works just fine, but sometimes when I power up the borad, I get this strange behaviour.