Hi.
I made Golden Image file ,
The created image file must be merged into the FW of the MCU and programmed with I2C.
( 5. FlashStream® File Format in the (slua801) document.)
By the way, the MCU I am using is STM32F412RGT6 with SRAM 256KB and Flash 1MB.
I think the memory is small to program by merging the 180KB image into FW.
So, I hope we use the df.fs file with a smaller file size. Are there any problems?
Do SREC file and df.fs file, bq.fs file have the same effect? Which of the three files should I use?
What is the difference between programming the smallest df.fs file and programming the largest srec file?
thank you.