Other Parts Discussed in Thread: UCC28056, UCC256404
Hi,
According to the "PFCLCSREVM034 User Guide" document, the maximum designed power is 12V/14A/168W.
The situation I'm currently encountering is:
It can start smoothly (stable) when the input is 110VAC and the load is 10.5A.It starts when the load exceeds 10.5A, and will shut down and restart after about 3 to 10 seconds.
It can start smoothly when the input is 220VAC and the load is 15A, without the above problems.
So I want to increase the maximum power to 180W, or even 200W?
1. What parts need to be changed?
2. Or is there any way to solve the problem of insufficient power at low voltage?
Best Regards