Part Number: LM22673
Other Parts Discussed in Thread: LM22672
I am using the LM22673. I use the part twice on one board, for 3.3V and for 5V output with an input voltage of 24V. Over the last 3 years I got more than 10 defect PCBs back from customer. Sometimes 3,3V is defect sometimes 5V is defect. Its always the Softstart pin (100nF), "damaged", means a short to ground (several Ohms up to 1k). Any recommendations to solve the issue?
see schematic R201 (56k) is not populated