Other Parts Discussed in Thread: TPS2117
Hi,
I'm using the manual mode with this chip, that both MODE and PRI1 are toggled by GPIOs. And I have several questions:
- May the IO signal level higher than both VIN1 and VIN2?
- I'm considering below conditions, which are not shown in the truth table. What's the VOUT in these situations?
- MODE = 1, PR1 = 1, VIN1 < 1.6V
- MODE = 1, PR1 = 0, VIN2 < 1.6V
Thanks.