This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Part Recommendation

Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65988, TPS25751, , TPS65987, TIDA-010047

On the Power Delivery side, we would probably use and external 100W PSU with USB-C, and we will consume probably 60 to 70 Watts.

Scenario 1 is that this plug would be exclusively to power our unit, while scenario 2 would be powering the unit (up to 100W) but also be able to give power up to 15W to external phone or device.

I have taken a look at your website, and the TPS65987D seems a good candidate.

 Can you confirm it will work? 

The second USB-C port would only be able to give 15W to an external device along with USB 2.0 and 3.1 data.

On this one, not sure if we limit to 5V only or 5V/9V… and which PD controller to choose from.

What device do you recommend?