This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25172: Output connected to TPS62840DLCR Step-Down Converter (without battery input)

Part Number: BQ25172
Other Parts Discussed in Thread: BQ24040,

Hi,

I've designed PCB where I'm charging battery using BQ25172DSGR (IC3) IC. I'm using TPS62840DLCR (IC5) IC to Step-Down Converter to power my MCU and other components.

Please find attached image of schematic.

When I don't connect battery at J8 connector, IC3 is not supplying proper output. due to this IC5 is not giving 3.3V output.

My application require to operate device if battery is not inserted and supply is coming directly from USB input.

Any solution for this which I can do in currret designed PCB.

Please suggest.