This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82903: Load transient by WEBENCH simulation

Part Number: TPSM82903

1. Vout=1.1V Iout=1.21A

   The result is shown in the figure below.

   Why doesn't the center reach 1.1V?

2. Vout=1.09V Iout=1.21A

   The result is shown in the figure below.

  There are two peaks on the right, is that correct?