This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: interfacing AFE with arduino and STM to make BMS

Part Number: BQ76940

i want to know about BQ76940 AFE....is it possible to connect with arduino for BMS monitoring? .......is there any readymade AFE board available like BQ76940EVM for connect and code by arduino

  • Hi Naveen,

    The bq76940 should be able to interface with an Arduino just like any other I2C peripheral. For ready-made boards, the only option we sell would be the bq76940EVM. We don't have a board designed specifically for an Arduino, but the EVM should support an external I2C connection.

    We don't have any pre-made code for the Arduino platform, so you will need to develop that yourself. I recommend referring to the MSP430 sample code (https://www.ti.com/lit/an/slva626b/slva626b.pdf).

    Regards,

    Max Verboncoeur

  • here am trying to make one circuit using TI BQ76940(as per datasheet connection) for communicate with arduino board.....i start it from scratch and also i have doubt about coding side also, how to boot this ic using arduino?...please share any reference ,if someone shared the related things how to code and read the complete things

  • Hi Naveen,

    You can boot the device by providing a high signal at the TS1 pin. I recommend referencing this application note for various ways of doing this: bq769x0 boot switch alternatives. The simplest would be to use a GPIO pin from the Arduino and a diode (Figure 1 of the app. note).

    For the software, we provide the sample code that I linked in my previous reply for customers to use as reference in their own software development.

    Regards,

    Max Verboncoeur