This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC5350-Q1: Capacitor size choose for Negative Bias curcuit used in SiC mos driving

Part Number: UCC5350-Q1
Other Parts Discussed in Thread: UCC5350

Hi,

     I see the negative bias curcuit example as UCC5350's spec shows below:

     So,how about setting the value of CA1 and CA2?

     Is there any suggestion?

  Regards

  Arrow

  • Hi Arrow,

    You need the series combination of these capacitors to be at least 20x the size of the input capacitance of the FET that is being driven. For example, IMZA75R020M1H has Ciss=2.2nF. C1 + series C2 be at least 44nF to drive this FET with this gate driver. 

    In addition, if these capacitors are the same size, you will have start-up transient voltages that are centered around "signal emitter", not scaled to the values set by the resistors. You can avoid this problem by scaling the capacitor divider to the right DC value.

    For a simple numerical example, say my target is >44nF in series, and my target voltages are -2V and +20V. My capacitor divider should be 1/21.

    CA1 could be 47nF, and

    CA2 could be 1uF

    to satisfy both requirements. Their series combination would be 44.9nF, and their scaling would be .9/20, which is close enough for this purpose.

    Best regards,

    Sean  

  • Hi Sean

    Thanks for your clarification. It's now totally clear to me now.

    Regards

    Arrow